项目支持

多年以来,Nanotec Electronic GmbH & Co. KG 一直在为高等院校和职业学院的科研项目 提供产品和专业技术支持。 
要获得资金支持 的科学项目 应当满足 下列条件:

  • 在课题/内容方面具有创新性,
  •  符合 科学工作的方法,
  • 能 对社会产生积极作用 。

 德国奖学金计划 旨在为来自世界各地成绩优秀并献身科学的学生提供财务和非物质支持。该奖学金采用公私合作原则,由企业、基金会或私人来赞助青年人才,每月承诺支付 150 欧元。而联邦政府将配套给予另外的 150 欧元。但在更多情况下:许多大学和私人赞助商也会通过并行的辅导项目、交流活动和实习机会来支持德国的奖学金获得者。

我们认为, 科学人才是德国未来经济发展 的中流砥柱,为他们提供支持是我们义不容辞的责任。因此,Nanotec Electronic 成为德国奖学金计划的资助商之一。

2017 年 德国奖学金颁奖现场
照片:Andreas Heddergott

The declared goal of the "Formula Students" is to design and build a race car within a year and drive it over the finish lines of Europe's racetracks. The e-gnition team of the TUHH (Technical University of Hamburg-Harburg) has successfully participated in this contest with its electrical race car every year since 2012. The team consists of almost 60 students from all TUHH degree programs. In 2017, they ranked 9th amongst participants with electric vehicles at the "Formula Student Germany” which takes place annually at the Hockenheimring race track.

New in 2017 was the driverless category, in which an existing vehicle is converted to a fully autonomous vehicle. In order to do this, the students used Nanotec's DB59S024035 brushless DC motor to rotate the steering shaft and thus steer the car autonomously. It replaces the hands of the driver who would normally turn the steering wheel.

The e-ignition team was delighted after the race, as their autonomously driving race car came in third in the world ranking of the "Autonomous Design Award".

Source and photos: Ole Ramming

Short video under https://youtu.be/2QbS5NKvrWg.

For 13 months, a team of 21 students from the University of Leuven in Belgium worked on the Punch 2, a new solar car with which they started in the Bridgestone World Solar Challenge in Australia on October 8. The race lead straight through the Australian Outback, from Darwin to Adelaide, over a distance of 3,000 km.

This year a lot of novelties have been put in the solar car. Among other features, the Punch 2 is equipped with a unique mechanical four-wheel steering system which consists of a mechanically decoupled front and rear wheel steering. This means that the front wheels rotate with the first 90° displacement of the steering wheel. When the driver continues to turn the steering wheel, the rear wheel steering is activated additionally. The steering motion is transferred to the four wheels using steel cables and nylon pulleys. 

Because this is a new and quite challenging concept, the team decided to build a copy of the steering system and perform tests with it before implementing the system in the solar car. A brushless DC servo motor from Nanotec was used in combination with a gearbox and linked to the steering wheel to simulate the steering movements during the race. The steering forces were simulated by using strong springs which required a gearbox to provide the required torque. 

Text and photos: Martijn Schaeken

慕尼黑应用科技大学机械电子/精密工程专业的学生为吉他拾音器开发了一台自动绕线机,并在今年夏季学期的“机电一体化”研讨会中亮相。 

他们开发了一种特殊的弹簧系统,使得漆包线在拾音器线轴上缠绕时不会卡住。为了驱动拾音器的旋转,他们采用了 NEMA 23 步进电机 ST5918。在 SMCI35 控制器的帮助下,可以在绕线数增加时让驱动电机的速度逐渐增加到某个阈值。然后电机以恒定速度旋转,直到绕线完成。 

此外,通过线性定位驱动器 LS20,线材可在线轴的整个宽度上平行于拾音器旋转轴连续馈送。

2016 年 5 月 14 日至 5 月 15 日,Ecorace 挑战赛第三期在比利时布鲁日举行。七个团队使用他们的比例模型参与比赛,争夺最具创新性船舶、最佳全能载货船、最佳全能非载货船和最佳商业计划奖项。

最具创新性船舶和最佳全能载货船的奖项都被鲁汶大学的“Galena”获得,这是一艘货船模型,用来运载一吨货物并在内陆航道航行。将来,Galena 应该能够完全自主航行。Nanotec 的  PD4-N5918L4204 被连接到变速箱  GPLE60-2S-16,作为这艘船的转向装置。

我们祝贺 Dominic Libanio、Christian Schorr 和 Pascal Lindemann 荣获“ “Jugend Forscht” 地区竞赛冠军以及莱茵兰-普法尔茨州创意竞赛第二名。这个得到 Nanotec 电机支持的项目旨在开发一款手部治疗仪器。

由于成本和时间因素导致运动疗法无论是在规定上还是在执行上,都无法到达所需的限度,所以手部在接受手术和后续治疗后通常无法达到最佳治疗效果。由此可能造成手指关节的基本运动受限,运动机能敏感性失常。这款手部治疗仪器将为医生和理疗医师提供支持。该仪器为每根手指提供可独立调节的机械机构,这些机械机构由 Nanotec 线性电机驱动。 

在柏林经济学院,应用工业电子专业的学生受托开发一款机器人,要求该机器人能够根据定制软件建造任意高度和形状的墙壁。 一个由机载 ATmega32 控制的几乎自主的无线运载工具在六个月之内建成。 这一运载工具由两个机载 Nanotec 步进电机驱动,每个电机带动一个轴装外部铝轮,实现精准位置控制。前后两个支撑架在增加该运载工具重量的同时,还能在运载工具行驶过程中来回滑动,从而确保稳定性。前部线性执行器推动一个手臂沿线性导轨上下移动。配备电磁铁的手臂可以提放木块,而木块则用金属板固定并放在预设位置。该运载工具由 12 伏锂聚合物电池供电。借助直观的用户界面,用户可以操控运载工具在基站和建筑工地之间行驶,最终建成高度不同的墙壁。

从 2009 年开始,德国盖尔森基兴市的威斯特伐利亚大学机械工程学院每年都会举行一次应用科学年度竞赛。每个参赛的学生团队都要开发出一台机器来完成特定任务。今年,他们接受的挑战是设计和制造用于冠形瓶塞的自动开瓶器,并对其进行编程。在开瓶之后,开瓶器还要将预定数量的饮料自动倒入玻璃杯中。2015 年度竞赛的获胜者是一个四人设计团队,他们选择了 Nanotec 的线性执行器 LS4118S1404-T6x2-75 来执行开瓶动作,而该线性执行器的更快速度和更高可靠性成为了他们获胜的决定性因素!

慕尼黑应用科技大学的机电一体化及精密机械项目模块旨在根据项目概念或现有项目来创造成品,其中包括演示和论证过程。2015 年夏季学期的学生设计了一款蠕动泵,每分钟能够恒定输出一升流体。这涉及到编写必要软件、建造泵并把它投入使用。该泵通过 Arduino Micro(一个包含微控制器、电源和电机驱动器等部件的电路板)控制。电机转速通过多孔圆盘检查并通过软件进行评估。Nanotec 步进电机充当了蠕动泵的软件和设计部件之间的接口。 

在吉森大学的应用戏剧研究学会,有一个 学生项目 是重建集市摊位游戏 “肯塔基赛马” 。在这个技巧游戏中,玩家要能够熟练操控比赛球来促使其机械马前往终点。与原型不同的是,新版本中的玩家不直接与游戏过程进行互动。相反,参赛者都坐在另外一个由摄像头监控的房间里面。玩家的热情越高,越能激励他的马快速跑向终点。例如,通过叫嚷或拍手,叫的越响、拍的越快,马跑的越快。这些马由 Nanotec 提供的步进电机 PD4-N6018L420 驱动。这些电机由相同的软件(光线和声音)控制,实现了机械元件和视听媒体的完美结合。

2014/15 冬季学期,卡尔斯鲁厄大学机电一体化专业的学生在项目研究中开发了一款曲棍球机器人。该机器人将取代一名玩家,与另一名玩家对战,它能完全自主行动,并根据游戏本身的情况作出决定。球的位置和速度由传感器系统获取,并由电子评估系统进行处理,随后数据被发送到机械控制推进器,使它可以移动到一个特定的位置将球击回。Nanotec 的步进电机用来移动与推进器相连的连接架。ST5918L4508 在该应用中提供恰当的转矩并由 SMCI35 控制器驱动。

来源和照片:Jakob Bokemeyer、Sergej Krohmer、Tobias Sperling、Urs Wetzel、SimonWörner、卡尔斯鲁厄应用科学大学

Nanotec Electronic 为奥格斯堡大学的 MALOMAT 项目提供支持。该项目将帮助残疾儿童凭自己的力量在画布上绘画。     

位于科尼格斯不伦的弗里茨-费尔森施泰因豪斯是一所为身体残疾和智力障碍儿童开设的学校。在这里,画画是课堂上 的重要内容。然而,孩子们并没有能力自己作画。在画画时,他们先选择一种颜色,告诉老师要涂抹在画布的哪个位置上。然后, 由老师将相应的颜料涂在所选 位置上。 

借助于 MALOMAT 项目,这些儿童可以自己或两人合作 在画布上画画。 他们可以选择三种不同颜色的线条,而且还可选择不同的难度。MALOMAT 项目使用了 Nanotec 赞助的一个齿轮电机和一个控制器。  

这个装置并不常见:用于产生风电的风筝。Nanotec 公司通过 SMCI36 和 SMCI35 步进电机控制系统支持八位巴登符腾堡双元制应用技术大学学生完成了这个 项目 。通过该项目,这些学生在 2011 年度“伽利略创新大赛”上获胜,荣膺欧洲最佳团队。